Electrification
The Trailblazer HP air-to-water heat pump provides both cooling and heating in a single efficient system. By absorbing heat from the ambient air or dissipating heat into it instead, the Trailblazer HP operates as an optimal chiller for both HVAC and industrial processes alike.
While the specific carbon footprint of an air-cooled heat pump chiller may vary depending on a region's electrical grid and the unit’s efficiency, replacing a building's fossil fuel heat sources with electrically powered alternatives, like Trailblazer HP, can provide building owners with additional ways of reducing the direct use of fossil fuels in their buildings.